About LDO for SNVS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About LDO for SNVS

跳至解决方案
731 次查看
Edgard
Contributor III

Dear an Engineer,

 

I'm wondering what LDO I should choose. 

On the RT1020 EVMK circuits, there is UM1750S-00. 
But UM1750S-00 is minor LDO, it is a little bit difficult to purchase in my country.

I have a question, dose "SNVS loard regulation" require the ability of max 350mA current?
I found other LDO and it was max 300mA current.

Thanks in advance.

标签 (1)
0 项奖励
1 解答
707 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Edgard ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   In fact, the MIMXRT1020-EVK is using the DCDC in default, although the LDO is added, but not used, you can see, the resistor to the LDO is DNP:

kerryzhou_0-1692599127320.png

So, if you use the DCDC like the EVK, LDO don't need to use:

kerryzhou_1-1692599150375.png

If you need to use the LDO for the SNVS,  300mA current is also too much larger, as you know, our SNVS is uA current, you also can select more smaller LDO.

kerryzhou_2-1692599233715.png

 

Wish it helps you!

Best Regards,

Kerry

 

 

在原帖中查看解决方案

0 项奖励
2 回复数
708 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Edgard ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   In fact, the MIMXRT1020-EVK is using the DCDC in default, although the LDO is added, but not used, you can see, the resistor to the LDO is DNP:

kerryzhou_0-1692599127320.png

So, if you use the DCDC like the EVK, LDO don't need to use:

kerryzhou_1-1692599150375.png

If you need to use the LDO for the SNVS,  300mA current is also too much larger, as you know, our SNVS is uA current, you also can select more smaller LDO.

kerryzhou_2-1692599233715.png

 

Wish it helps you!

Best Regards,

Kerry

 

 

0 项奖励
702 次查看
Edgard
Contributor III
Dear Kerry

thanks for your advice.
I could understand. I'll try to design the circuits without LDO.

Kindest Regards
Edgard