About LDO for SNVS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About LDO for SNVS

Jump to solution
733 Views
Edgard
Contributor III

Dear an Engineer,

 

I'm wondering what LDO I should choose. 

On the RT1020 EVMK circuits, there is UM1750S-00. 
But UM1750S-00 is minor LDO, it is a little bit difficult to purchase in my country.

I have a question, dose "SNVS loard regulation" require the ability of max 350mA current?
I found other LDO and it was max 300mA current.

Thanks in advance.

Labels (1)
0 Kudos
1 Solution
709 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Edgard ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   In fact, the MIMXRT1020-EVK is using the DCDC in default, although the LDO is added, but not used, you can see, the resistor to the LDO is DNP:

kerryzhou_0-1692599127320.png

So, if you use the DCDC like the EVK, LDO don't need to use:

kerryzhou_1-1692599150375.png

If you need to use the LDO for the SNVS,  300mA current is also too much larger, as you know, our SNVS is uA current, you also can select more smaller LDO.

kerryzhou_2-1692599233715.png

 

Wish it helps you!

Best Regards,

Kerry

 

 

View solution in original post

0 Kudos
2 Replies
710 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Edgard ,

   Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.

   In fact, the MIMXRT1020-EVK is using the DCDC in default, although the LDO is added, but not used, you can see, the resistor to the LDO is DNP:

kerryzhou_0-1692599127320.png

So, if you use the DCDC like the EVK, LDO don't need to use:

kerryzhou_1-1692599150375.png

If you need to use the LDO for the SNVS,  300mA current is also too much larger, as you know, our SNVS is uA current, you also can select more smaller LDO.

kerryzhou_2-1692599233715.png

 

Wish it helps you!

Best Regards,

Kerry

 

 

0 Kudos
704 Views
Edgard
Contributor III
Dear Kerry

thanks for your advice.
I could understand. I'll try to design the circuits without LDO.

Kindest Regards
Edgard