ADC accuracy on first read

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC accuracy on first read

701 Views
GuillaumeAudirac
NXP Employee
NXP Employee

Using i.MXRT1062, the first ADC value is slightly lower than the expectation.

Settings:

  • Software Triggering
  • 12 bits ADC resolution

The starting sequence (using fsl_adc):

  1. ADC_Init()
  2. ADC_EnableHardwareTrigger()
  3. ADC_DoAutoCalibration()
  4. In loop, at key press:
    1. ADC_SetChannelConfig()
    2. Wait for ADC_GetChannelStatusFlags
    3. ADC_GetChannelConversionValue() at key press

Outputs:

  • First value read: ~3200
  • Following value read: ~3400-3450

Do you have any idea why the first value is not accurate ?

Thanks.

(sample code attached)

Guillaume Audirac
Tags (2)
0 Kudos
1 Reply

557 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Guillaume Audirac,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I've not replicated this phenomenon that you described, during the testing, I run the ADC demo to sample the Gnd, DCDC_3V3, and DCDC_OUT respectively.

pastedImage_1.png

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos