ADC Accuracy Issue for Low Voltage Readings on RT1176.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Accuracy Issue for Low Voltage Readings on RT1176.

187件の閲覧回数
Pavankumar1
Contributor II

Hello,

I am using the ADC in the RT1176 controller with a 1.8V reference voltage. I am able to read values above 15.2mV correctly, but values below 15.2mV are not read accurately. Could you please help me understand what might be causing this issue and what the minimum value is that the ADC can reliably read?

Thank

タグ(3)
0 件の賞賛
返信
1 返信

137件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @Pavankumar1 ,

Thanks for your interest in NXP MIMXRT series!

NXP doesn't provide information on the minimum readable value of the RT1170 ADC, but according to the design specification of the ADC, the results you mentioned are unlikely to occur. The error will not be as large as the one you have tested because it is based on its LSB. The error can be minimized by calibrating the application before testing and averaging multiple measurements. It is also recommended to test with an official EVK first to rule out hardware effects.

Best regards,
Gavin

0 件の賞賛
返信