i.MXRT1170-EVK LPUART idle line interrupt with EDMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MXRT1170-EVK LPUART idle line interrupt with EDMA

跳至解决方案
1,084 次查看
igrinberg
Contributor II

Hi,

I would like to use the LPUART of the EVK board to receive messages of unknown size.

For this purpose, I would like to combine the usage of idle line interrupt and the eDMA mechanism.

The examples found in the SDK are with IRQ separately and eDMA separately, how can I combine the two?

Is there a relevant example code?

Thanks,
Ira.

 

0 项奖励
回复
1 解答
1,066 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

You can use the example "lpuart_edma_rb_transfer" from the RT10xx SDKs as a reference for Idle Line Detection.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,067 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

You can use the example "lpuart_edma_rb_transfer" from the RT10xx SDKs as a reference for Idle Line Detection.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复