i.MX RT1010 CRC driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1010 CRC driver

ソリューションへジャンプ
1,312件の閲覧回数
mhanuel
Contributor II

I cannot find an example or the driver to do CRC on i.MX RT1010.

I understand the processor is capable of with a Data Co Processor but the only information is a short description on RM section 7.5.

Can someone please help clarify?

Many thanks,

Manuel

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,273件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Manuel, 

In version 2.8.0 of the SDK, you will find an example named DCP. This example project has a CRC32 test for the DCP engine. Also, in the RT1010 security reference manual, you will find more information about the CRC32. You can request this document in the following link

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,274件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Manuel, 

In version 2.8.0 of the SDK, you will find an example named DCP. This example project has a CRC32 test for the DCP engine. Also, in the RT1010 security reference manual, you will find more information about the CRC32. You can request this document in the following link

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

0 件の賞賛
返信