i.MX RT internal LDO and DC/DC converter's specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT internal LDO and DC/DC converter's specification

855件の閲覧回数
masahirokiniwa
Contributor IV

I checked the data sheet and reference manual for i.MX RT 1050, but I couldn't find some specifications.

Could you tell me below specifications?

<DC/DC converter>

 - Switching frequency

 - Radiation noise on the reference circuit (i.MX RT1050 EVK)

<LDO>

 - PSRR : Power Supply Rejection Ratio

If I can find them by other documents, could you tell me them?

Best regards,

M.Kiniwa

タグ(1)
0 件の賞賛
返信
1 返信

765件の閲覧回数
art
NXP Employee
NXP Employee

Q. Switching frequency

A. The typical switching frequency of the i.MX RT1050 DCDC converter is 1.6MHz.

Q. Radiation noise on the reference circuit (i.MX RT1050 EVK)

A. Not specified.

Q. PSRR : Power Supply Rejection Ratio

A. Not specified. The only parameter specified here is the LDO output accuracy that is +/- 25mV.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信