What is the recommended SEMC operation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the recommended SEMC operation?

1,759 Views
george
Senior Contributor II

Dear All,

Now we want to use SEMC to connect i.MX-RT1050 and FPGA.

The interface to FPGA is considering general parallel connection using address lines and data lines.

It is an interface where address lines and data lines are completely separated.

It has almost the same interface as legacy SRAM and parallel NOR-flash.

*For example : http://www.issi.com/WW/pdf/IS29GL256_128.pdf 

In the i.MX RT1050 processor reference manual, the NOR flash interface seems to be appropriate.

However, in this community post, the Pseudo SRAM interface is often chosen for some reason.

Should we choose Pseudo SRAM interface too?

Theare is another question.

This is a common question for NOR interface and pseudo SRAM interface.

What is the COL(column address bit width) in NOR/SRAM control register 0 ?

BR,

George

Tags (1)
0 Kudos
Reply
3 Replies

1,546 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Use recommended signals connection table in section 25.4.3 (Pin Mux in SEMC) in the
Reference Manual for NOR / SRAM.

 https://www.nxp.com/webapp/Download?colCode=IMXRT1050RM 

  Bit field COL of SRAM control register 0 (SRAMCR0) is not used, may be zero.

Burst Length BL bit field should be zero.

Regards,

Yuri.

0 Kudos
Reply

1,546 Views
george
Senior Contributor II

Dear Yuri‌,

Thank you for your replay.

NORCR0 COL and BL should be zero like SRAMCR0, right?

BR,

George

0 Kudos
Reply

1,546 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Correct -  for NOR as for SRAM.

Regards,

Yuri.

0 Kudos
Reply