Using NAND flash on iMX RT 1170 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using NAND flash on iMX RT 1170 evk

Jump to solution
1,993 Views
FaroukBouabid
Contributor I

Hi, I am trying to use the NAND flash through SEMC on the iMX RT 1170 evaluation board and I couldn't help but notice that the resistors on the nand_data pins are not integrated. Is there a hardware modification that must be performed on this board in order to use the NAND flash and SDRAM in the same time ? Thx in advance, Best regards.

0 Kudos
Reply
1 Solution
1,976 Views
jay_heng
NXP Employee
NXP Employee

NAND flash device is not enabled by default on RT1170 EVK board, you need to populate R1872~R1879 to enable NAND. and I have ever done NAND boot time test on EVK (https://www.cnblogs.com/henjay724/p/12591382.html)

As NAND device shares some same SEMC signals with SDRAM device (but with different CS), so it is not easy to use them in some case (for example, copying page data from NAND to SDRAM directly via AHB bus), but below case is ok:

NAND stores user application, after bootup, BootROM copies application from NAND to TCM, then application executes in TCM and configures SEMC to use SDRAM

View solution in original post

0 Kudos
Reply
5 Replies
1,977 Views
jay_heng
NXP Employee
NXP Employee

NAND flash device is not enabled by default on RT1170 EVK board, you need to populate R1872~R1879 to enable NAND. and I have ever done NAND boot time test on EVK (https://www.cnblogs.com/henjay724/p/12591382.html)

As NAND device shares some same SEMC signals with SDRAM device (but with different CS), so it is not easy to use them in some case (for example, copying page data from NAND to SDRAM directly via AHB bus), but below case is ok:

NAND stores user application, after bootup, BootROM copies application from NAND to TCM, then application executes in TCM and configures SEMC to use SDRAM

0 Kudos
Reply
1,974 Views
FaroukBouabid
Contributor I

Thanks for your reply. As a particular use case, is using the NAND flash as a data storage media and the SDRAM for the application acceptable ?

Tags (1)
0 Kudos
Reply
1,970 Views
jay_heng
NXP Employee
NXP Employee

CPU fetches app instruction from SDRAM while app wants to read data from NAND via the same SEMC DQ[x:0], it is kind of hard to manage this case but SEMC supports it in theory.

0 Kudos
Reply
1,968 Views
FaroukBouabid
Contributor I

Isn't Queue B supposed to manage SDRAM when A is overloaded with NAND requests ? (By application I didn't mean code : I meant data (Heap - stack))

0 Kudos
Reply
1,953 Views
jay_heng
NXP Employee
NXP Employee

I just checked this case with SEMC designer, he said that this case was well supported by SEMC.

0 Kudos
Reply