Undocumented Changes in Documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Undocumented Changes in Documentation

387 Views
Stephan_
Contributor I

Hi,

I'm working with RT1176 and have observed undocumented changes in reference manual IMXRT1170RM. As example in Version Rev. 2, 06/2023 in register description for SW_PAD_CTL_PAD_GPIO_LPSR_04 the description of SRE bit tells:

0b - Slow Slew Rate
1b - Fast Slew Rate

And in Version ev. 1, 05/2021 the description for same bit is:

0 - Fast Slew Rate
1 - Slow Slew Rate

I can't see this change in history or errata. Is there any way to get in touch with such changes except diff over hole documentation.

0 Kudos
Reply
1 Reply

367 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

Changes to the document are available in the revision history unfortunately it is not listed in that appendix as it is considered "No substantive change".

It is important to clarify that the correct value for this field is the one from rev2 as it matches with the code generated with config tools.

Best regards,
Omar

0 Kudos
Reply