Storing user data to QSPIFlash running in XIP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Storing user data to QSPIFlash running in XIP

1,489 Views
chekurianemarid
Contributor I

 Hi

I trying to store user data to QSPI Flash(IS25LP128F) after code area which is connected to IMXRT1050. My application is running from flash in XIP mode.

I tried the solutions( https://www.nxp.com/docs/en/application-note/AN12564.pdf ) and reference code(https://www.nxp.com/docs/en/application-note-software/AN12564SW.zip ). Reference from flexspi_rww.c implementation  iam able to read vendorid(flexspi_nor_get_vendor_id(EXAMPLE_FLEXSPI, &vendorID)),Entering into Quad mode( flexspi_nor_enable_quad_mode(EXAMPLE_FLEXSPI)),Erase sector(flexspi_nor_flash_erase_sector(FLEXSPI,SECTOR)) in single step mode while debugging but in free flow of application run the application is crashing.

is what iam trying is correct.is there any other solution. 

Note : Iam trying to use same QSPI Flash chip to store both application code and  user data storing.

Regards

venu

Labels (1)
0 Kudos
Reply
3 Replies

1,211 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, venu 

The approach explained on the AN12564 application note, is recommended when you have two different memories, one for the code and one for user data. Since in your case you are using the same QSPI flash chip to store your application and user data, your best option is to allocate the flash write/erase/read functions to other memory(except currently writing flash, generally allocate to internal SRAM). The following community document, explains how to do this with MCUXpresso IDE. 


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,211 Views
chekurianemarid
Contributor I

HI,

Thanks for the reply.I could not find the link to the community document that you are referring to.Can you please resend the link for the document. 

0 Kudos
Reply

1,211 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, venu 

Sorry, I forgot to put the link in my previous reply.

https://community.nxp.com/thread/389110 

Regards,

Victor 

0 Kudos
Reply