Re: booting related imxrt117x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: booting related imxrt117x

Jump to solution
1,674 Views
aravindhg
Contributor II

booting related imxrt117x  
@Pavel_Hernandez
Hi,
please follow our previous query ....
I am attaching previous thread above iMXRT1170 ,#iMXRT117x

 we are using the following :
1.QSPI based winbond external flash.
2.Yes, but we are facing issues in the newly designed card which is almost similar to our old card.
3.fuses burned as per internal boot mode.
4.boot config and boot mode are internal boot mode.
5. we are using the SWD
6.MCUxpresso link debugger
7. we are using the latest version of MCUxpresso 11.6
8.communication with external flash is not sure, controller is unable to load the code into QSPI flash

I am attaching details again the same.
Regards,
Aravindh.

0 Kudos
Reply
1 Solution
1,646 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I reviewed your case, and this is a duplicate could you close this I will continue the support in the other.

Best regards,
Pavel

View solution in original post

0 Kudos
Reply
1 Reply
1,647 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I reviewed your case, and this is a duplicate could you close this I will continue the support in the other.

Best regards,
Pavel

0 Kudos
Reply