RT1176 Inductor for the internal DC-DC Converter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1176 Inductor for the internal DC-DC Converter

374 Views
Wobaffet
Senior Contributor I

Hello, 

For our project, we'll be using RT1176 MCU, on the design for the evk there is a 4.7uH inductor which is this: 74404041047 from würth. Instead of this can we use one of the alternatives below?

SRP0420-4R7K from Bourns Inc.

DFE322520FD-4R7M=P2 from Murata

Thank you in advance!

Best Regards.

0 Kudos
Reply
1 Reply

350 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

NXP does not recommend any component that is not an NXP product. The recommended value for the external inductor is about 4.7 μH with the saturation current > 1.5 A and ESR < 0.1 Ω.

Hope it helps you.

Have a nice day!

0 Kudos
Reply