RT1170 custom bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1170 custom bootloader

688 次查看
sandeepc
Contributor IV

Hi,

I want develop custom boot loader using Qspi external flash.

 

If you have any better document to understand the memory organization to implementation of boot loader please shar with me.

processor: imxrt1170

External flash: winbond(W25Q64JV)

Mode: XIP mode

Regards,

Sandeep C

@kerryzhou 

0 项奖励
回复
6 回复数

580 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @sandeepc ,

  About the bootloader, we have a lot of codes for your reference.

1. SBL/SFW

https://www.nxp.com/docs/en/user-guide/MCUOTASBLSFWUG.pdf

2. sdk

https://mcuxpresso.nxp.com/en/builder?hw=MIMXRT1170-EVK

\SDK_2_15_000_MIMXRT1170-EVK\boards\evkmimxrt1170\ota_examples

About the flash operation, you can refer to SDK:

SDK_2_15_000_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\fsl_romapi

SDK_2_15_000_MIMXRT1170-EVK\boards\evkmimxrt1170\driver_examples\flexspi\nor

 

Wish it helps you!

If you still have question about it, please kindly let me now.

If your question is solved, please help to mark the correct answer, just to close this case, thanks.

Best Regards,

Kerry

0 项奖励
回复

564 次查看
sandeepc
Contributor IV
Thanks for the reply.
i will refer...

683 次查看
Bkaya
Contributor III

Hi @sandeepc ,

You can use SDK example bootloader or i shared link below that i used while designing my bootloader project. I can not share my code but if you have any question i want to help.

Best Regards,

Basri KAYA

 

https://github.com/NXP/mcu-smhmi

0 项奖励
回复

678 次查看
sandeepc
Contributor IV
Thanks,
i will go through your code.

Do you have any document to understand well xip boot?

Regards,
Sandeep c

Regards,
sabdeep C
0 项奖励
回复

669 次查看
Bkaya
Contributor III

You are welcome. That is not my code but it will be very usefull to start writing your code.

For Xip Boot, you can import SDK example romapi_cm7 for 1170.

0 项奖励
回复

666 次查看
sandeepc
Contributor IV
Ok, thanks i will go through your code.
Regards,
Sandeep C
0 项奖励
回复