RT1052 on/off pin explanation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052 on/off pin explanation

Jump to solution
1,670 Views
variable_andrew
Senior Contributor I

I'm trying to understand the on/off pin connectivity and functionality requirements.

 

The confusing thing in the RT1052's RM is the mention of an external PMIC, does this mean the ONOFF pin can't just be directly connected to a user button and held down to effectively 'shut down' the RT1052?

1.

In section 13.5 of the RM, it sounds like if you just connect the ON/OFF button to a button it'd work as per the state diagram (fig 13-10), but then it mentions connecting to a PMIC/voltage regulator, making it sound like ON/OFF is actually an output that controls the voltage regulator?

 

2.

in "off" state, does the device basically act the same as if it was programmatically put into SNVS mode ?

 

0 Kudos
Reply
1 Solution
1,646 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

1. ONOFF signal is an input for the RT. In section 13.5 of the reference manual, when we mentioned the following: The ONOFF logic inside of SNVS_LP allows for connecting directly to a PMIC or other
voltage regulator device. It means that you could connect a signal from the PMIC directly to the ONOFF pin to turn OFF the RT when the supply voltage goes away or drops below a certain level. 

2. Yes, when you turn OFF the RT with the ONOFF button it's the same is at it you send it to SNVS mode by software. 

 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

View solution in original post

3 Replies
1,647 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

1. ONOFF signal is an input for the RT. In section 13.5 of the reference manual, when we mentioned the following: The ONOFF logic inside of SNVS_LP allows for connecting directly to a PMIC or other
voltage regulator device. It means that you could connect a signal from the PMIC directly to the ONOFF pin to turn OFF the RT when the supply voltage goes away or drops below a certain level. 

2. Yes, when you turn OFF the RT with the ONOFF button it's the same is at it you send it to SNVS mode by software. 

 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

1,642 Views
variable_andrew
Senior Contributor I

got it, thanks @victorjimenez 

0 Kudos
Reply
1,653 Views
variable_andrew
Senior Contributor I

trying to bump this post up for some confirmation of my understanding.

0 Kudos
Reply