RT1050 POR_B issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 POR_B issue

805 Views
cyesman
Contributor II

RT1051 POR_B pin combined with a RESET IC(Push-Pull). Jlink cannot find the core. When I changed the RESET IC to Open Drain type, it's OK. I couldn't figure out why?

Labels (1)
0 Kudos
Reply
1 Reply

765 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Depends on the RM that POR_B must remain low (asserted) until the VDD_SOC supplies are stable.  But a RESET IC(Push-Pull) should be Active high. So can't meet MCU reset.

Have a nice day.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply