Max MIC Connection on SAI1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Max MIC Connection on SAI1

1,230 Views
vaidehi_patel
Contributor II

Hi Team,

For the i.MX RT 1060 design, can we connect 2 MICs for one single data line and clock with SAI interface from HW and SW perspective. And could this be repeat for 4 data lines with one single clock line i.e. 8 MICs in SAI interface.

One of the application note screenshot attached.

Than you in advance.

6 Replies

1,080 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, Vaidehi

The implementation you put on the image is possible with the RT1060. Unfortunately, we don't have an example that meets this implementation, however, you can take one of the SDK examples and use it as a base for your project. 

Regards, 

Victor 

1,080 Views
vaidehi_patel
Contributor II

Hello Victor,

Could you please also help for my another query wrt firmware/software support?

Please do the needful.

Regards,

Vaidehi

0 Kudos
Reply

1,079 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, Vaidehi

Unfortunately, we don't have an example that meets your implementation, however, you can take one of the SDK examples and use it as a base for your project. You can download the SDK  from the following link: Welcome | MCUXpresso SDK Builder 

Regards, 

Victor 

0 Kudos
Reply

1,079 Views
vaidehi_patel
Contributor II

Thank you Victor for the quick reply. This shall be useful to us.

0 Kudos
Reply

1,080 Views
vaidehi_patel
Contributor II

Hi,

On top of above que, could you please also share the Firmware/Software support from your end.

As mentioned, Amazon FreeRTOS will be provided. Is there anything else, you guys will be providing.?

Hoping for the quick response.

Thank you,

Vaidehi

0 Kudos
Reply

1,080 Views
vaidehi_patel
Contributor II
As discussed over mail,
Application is for Voice DSP processor design which should support Alexa voice services (WuW) with below features:
   -   Voice processing to clean up signal for better noise recognition
   -   Echo cancellation, Beamforming, source tracking, noise cancellation, AEC
Voice input should be given to MIC Array and output should be received from speaker.
We have purchased MCU based solution for AVS board for PoC.
As mentioned for MCU based solution for AVS design, Amazon FreeRTOS will be provided.
Could you please help, how to flash and boot-up the board?
Thank you in advance.
Regards,
Vaidehi
0 Kudos
Reply