MX RT1060 - target application software deployment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX RT1060 - target application software deployment

649 Views
jackking
Senior Contributor I

I posted a similar thread asking about how to handle end-user updating.  This would be on a custom board (not the EVK) and using something less complicated for the user than JTAG or MfgTools.  I assume the MCUboot/Flashloader can be wrapped in a user friendly desktop app for a dedicated device, it would only require USB connectivity (?)

0 Kudos
Reply
1 Reply

575 Views
Yuri
NXP Employee
NXP Employee

Hello,

  generally - yes, the i.MX RT flashloader  can be used to flash applications for the i.MX RT,

using only i.MX RT USB OTG port.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply