Hi Dear Authorized,
I have some cards which is lost debug connection. I am not able to connect my cards. These are specifically designed cards which uses RT1024 and RT1064. I am trying to recover them by MCUXpresso Secure Provisioning Tool. I want to use it by using UART.
Firstly, I tried this recovery operation with EVK a setup below. I am able to debug my card with this setup. I mean USB connections work but MCUXpressoSPT is not detecting my EVK. I don't know the official way of using UART SPT Mass Erase.
Could you direct me to the official way to do this?
My Setup and Details:
Thanks and Regards.
已解决! 转到解答。
I find extra informations below:
You can use above configurations with simple RS485-Serial connection.
RT1024 supports UART1-UART2 according to technical data.
RT1064 supports only UART1 according to technical data.
I am able to connect just over UART1 for both RT1024 and RT1064.
Thanks and Regards.
I find extra informations below:
You can use above configurations with simple RS485-Serial connection.
RT1024 supports UART1-UART2 according to technical data.
RT1064 supports only UART1 according to technical data.
I am able to connect just over UART1 for both RT1024 and RT1064.
Thanks and Regards.