MCUXpresso Secure Provisioning Tool - Mass Erase by UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Secure Provisioning Tool - Mass Erase by UART

Jump to solution
3,160 Views
Lukas_Frank
Senior Contributor I

Hi Dear Authorized,

 

I have some cards which is lost debug connection. I am not able to connect my cards. These are specifically designed cards which uses RT1024 and RT1064. I am trying to recover them by MCUXpresso Secure Provisioning Tool. I want to use it by using UART.

Firstly, I tried this recovery operation with EVK a setup below. I am able to debug my card with this setup. I mean USB connections work but MCUXpressoSPT is not detecting my EVK. I don't know the official way of using UART SPT Mass Erase.

 

Could you direct me to the official way to do this?

 

My Setup and Details:

  • LPUART1
  • FTDI Module
  • PmodRS485
  • Type-C USB Convertion HUB for Mac.
  • MCUXpresso IDE v11.8.0
  • MCUXpresso Secure Provisioning Tool v7

 

Lukas_Frank_0-1691921916619.jpeg

Lukas_Frank_0-1691669757076.png

 

 

Thanks and Regards.

0 Kudos
Reply
1 Solution
2,757 Views
Lukas_Frank
Senior Contributor I

I find extra informations below:

 

Lukas_Frank_0-1692364608268.pngLukas_Frank_1-1692364637867.png

 

 

You can use above configurations with simple RS485-Serial connection.

 

RT1024 supports UART1-UART2 according to technical data.

RT1064 supports only UART1 according to technical data.

 

I am able to connect just over UART1 for both RT1024 and RT1064.

 

 

Thanks and Regards.

View solution in original post

0 Kudos
Reply
21 Replies
2,758 Views
Lukas_Frank
Senior Contributor I

I find extra informations below:

 

Lukas_Frank_0-1692364608268.pngLukas_Frank_1-1692364637867.png

 

 

You can use above configurations with simple RS485-Serial connection.

 

RT1024 supports UART1-UART2 according to technical data.

RT1064 supports only UART1 according to technical data.

 

I am able to connect just over UART1 for both RT1024 and RT1064.

 

 

Thanks and Regards.

0 Kudos
Reply