MAC to MAC in RT1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MAC to MAC in RT1064

101 Views
chhsu0229
Contributor II

Hi,

I am working on a project that the RT1064 ENET connect to a Ethernet Switch (IP175D)through EMII mode and MAC to MAC  connection. The connection is below, I have modified the phy library and test the "dhcp_start()" function to send the enet command to network. 

I got the waveform form the wires. It seemd the RT1064 can not to decode the received signal from the IP175D.

How can I fix these issue?

111.jpg

0 Kudos
Reply
1 Reply

68 Views
Sam_Gao
NXP Employee
NXP Employee

Hi @chhsu0229 

Please check below comments

1. it is normal MAC without any RMII feature for RT1064, please check if this Switch(IP175D) support ReverseMII or not.

2. Please check the spec of IP175D to double confirm the hardware connection is correct, sometimes it may be reversed at the MAC-2-MAC connection.

3. Please check the send data, Can the Switch get the dhcp discover function?

 

BR.

Sam

0 Kudos
Reply