IMXRT1064 SEMC-SRAM with FPGA Data Corruption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1064 SEMC-SRAM with FPGA Data Corruption

264 Views
Lukas_Frank
Senior Contributor I

Hi Dear Authorized,

 

I am trying to create a SRAM Application with SEMC. The slave (opponent side) of IMXRT is a FPGA. I am writing sequential data with attached code as you seen in my memory browser monitor.

 

The Memory Browser Monitor:

Transmitted by IMXRT1064: 0x0000_0000, 0x0000_0002, 0x0000_0004, 0x0000_0006 ....

Lukas_Frank_0-1690274547667.png

 

The Data Acquired by FPGA:

Received by FPGA: 0xFFDF_0000 , 0xFFFF_0002, 0xFFDF_0004, 0xFFDF_0006 .... 

 

I am curious about why the data is acquiring in corrupted order in FPGA Side. We are monitoring FPGA data in logic analyzer.

 

I just tried different things checked connection pins everything looks ok. I can't understand where the problem is.

 

Is there a possibility to corrupt data which caused by my code even if data seen correct in memory monitor window?

 

My Code:

#include "fsl_debug_console.h"
#include "fsl_device_registers.h"
#include "pin_mux.h"
#include "clock_config.h"
#include "board.h"
#include "fsl_semc.h"

/*******************************************************************************
 * Definitions
 ******************************************************************************/
#define EXAMPLE_SEMC               SEMC
#define EXAMPLE_SEMC_START_ADDRESS (0x90000000U)
#define EXAMPLE_SEMC_START_ADDRESS_TX (0x900000A0U)
#define EXAMPLE_SEMC_START_ADDRESS_RX (0x900000B0U)
#define EXAMPLE_SEMC_CLK_FREQ      CLOCK_GetFreq(kCLOCK_SemcClk)

#define SEMC_EXAMPLE_DATALEN    16//(0x1000U)
#define SEMC_EXAMPLE_WRITETIMES (1000U)

/*******************************************************************************
 * Prototypes
 ******************************************************************************/
extern status_t BOARD_InitSEMC(void);
/*******************************************************************************
 * Variables
 ******************************************************************************/

uint32_t sram_writeBuffer[SEMC_EXAMPLE_DATALEN];
uint32_t sram_readBuffer[SEMC_EXAMPLE_DATALEN];

/*******************************************************************************
 * Code
 ******************************************************************************/

void SEMC_SRAMWrite32Bit_TXDREG(void);
void SEMC_SRAMRead32Bit_RXDREG(void);

status_t BOARD_InitSRAM(void)
{
    semc_config_t config;
    semc_sram_config_t sram_config;
    uint32_t clockFrq = EXAMPLE_SEMC_CLK_FREQ;

    /* Initializes the MAC configure structure to zero. */
    memset(&config, 0, sizeof(semc_config_t));
    memset(&sram_config, 0, sizeof(semc_sram_config_t));

    /* Initialize SEMC. */
    SEMC_GetDefaultConfig(&config);
    config.dqsMode = kSEMC_Loopbackdqspad; /* For more accurate timing. */
    SEMC_Init(SEMC, &config);

    //config SRAM
    sram_config.cePinMux           = kSEMC_MUXA8;        	// SEMC_ADDR08 is CE0# (IOCR[MUX_A8])
    sram_config.address            = SRAM_BASE;          	// Base address 0x90000000 (BR6[BA])
    sram_config.memsize_kbytes     = 0x10000;			// SRAM0 space size 64MB (BR6[MS])
    sram_config.addrPortWidth      = 8;                    	// Port width (SRAMCR0[COL]) Don't care in SRAM.
    sram_config.advActivePolarity  = kSEMC_AdvActiveLow;   	// ADV# polarity (SRAMCR0[ADVP]) Don't care if not use ADV.
    sram_config.addrMode           = kSEMC_AddrDataNonMux; 	// Non Mux mode (SRAMCR0[AM])
    sram_config.burstLen           = kSEMC_Nor_BurstLen1;	// Burst length (SRAMCR0[BL])
    sram_config.portSize           = kSEMC_PortSize16Bit;	// Port size 16bit (SRAMCR0[PS])
    sram_config.syncMode           = kSEMC_SyncMode;		// ASYNC mode (SRAMCR0[SYNCEN])
    //sram_config.waitEnable       = true;			// WAIT enable (SRAMCR0[WAITEN])
    //sram_config.waitSample       = 0; 			// WAIT sample (SRAMCR0[WAITSP])
    //sram_config.advLevelCtrl     = kSEMC_AdvHigh; 		// ADV# level control (SRAMCR0[ADVH]) Don't care if not use ADV.
    sram_config.tCeSetup_Ns        = 20; 			// CE# setup time [nsec] (SRAMCR1[CES]) Need tuning.
    sram_config.tCeHold_Ns         = 20;			// CE# hold time [nsec] (SRAMCR1[CEH]) Need tuning.
    sram_config.tCeInterval_Ns     = 20; 			// CE# interval time [nsec] (SRAMCR2[CEITV]) Need tuning.
    sram_config.readHoldTime_Ns    = 20; 			// Read hold time [nsec] (SRAMCR2[RDH]) Only for SYNC mode.
    sram_config.tAddrSetup_Ns      = 20; 			// ADDR setup time [nsec] (SRAMCR1[AS]) Need tuning.
    sram_config.tAddrHold_Ns       = 20;			// ADDR hold time [nsec] (SRAMCR1[AH]) Need tuning.
    sram_config.tWeLow_Ns          = 20; 			// WE low time [nsec] (SRAMCR1[WEL]) Need tuning.
    sram_config.tWeHigh_Ns         = 20; 			// WE high time [nsec] (SRAMCR1[WEH]) Need tuning.
    sram_config.tReLow_Ns          = 20; 			// RE low time [nsec] (SRAMCR1[REL]) Need tuning.
    sram_config.tReHigh_Ns         = 20;			// RE high time [nsec] (SRAMCR1[REH]) Need tuning.
    sram_config.tTurnAround_Ns     = 20; 			// Turnaround time [nsec] (SRAMCR2[TA]) Need tuning but don't set it to be 0.
    sram_config.tAddr2WriteHold_Ns = 20;			// Address to write data hold time [nsec] (SRAMCR2[AWDH]) Need tuning.
    sram_config.tWriteSetup_Ns     = 20; 			// Write Data setup time [nsec] (SRAMCR2[WDS]) Only for SYNC mode.
    sram_config.tWriteHold_Ns      = 20; 			// Write Data hold time [nsec] (SRAMCR2[WDH]) Only for SYNC mode.
    sram_config.latencyCount       = 20; 			// Latency count (SRAMCR2[LC]) Only for SYNC mode.
    sram_config.readCycle          = 20; 			// read time (SRAMCR2[RD]) Only for SYNC mode.
    //sram_config.delayChain       = 20; 			// typically not used in SRAM. (DCCR [SRAMXVAL], DCCR [SRAMXEN], DCCR [SRAM0VAL], DCCR [SRAM0EN])

    return SEMC_ConfigureSRAM(SEMC, &sram_config, clockFrq);
}

#if defined(CACHE_MAINTAIN) && CACHE_MAINTAIN
#include "fsl_cache.h"
#endif


int main(void)
{
    /* Hardware initialize. */
    BOARD_ConfigMPU();
    BOARD_InitBootPins();
    BOARD_InitBootClocks();


    CLOCK_InitSysPfd(kCLOCK_Pfd2, 29);
    CLOCK_SetMux(kCLOCK_SemcMux, 1);
    CLOCK_SetDiv(kCLOCK_SemcDiv, 7);

    BOARD_InitDebugConsole();

    if (BOARD_InitSRAM() != kStatus_Success)
    {
        PRINTF("\r\n SEMC SRAM Init Failed\r\n");
    }

    SEMC_SRAMWrite32Bit_TXDREG();

    return 0;
}

void SEMC_SRAMWrite32Bit_TXDREG(void)
{
    uint32_t index;
    uint32_t datalen = SEMC_EXAMPLE_DATALEN;
    uint32_t *sram  = (uint32_t *)EXAMPLE_SEMC_START_ADDRESS;

    for (index = 0; index < datalen; index++)
    {
        sram[index] = index * 2;
    }

}

 

Thanks and Regards. 

Labels (1)
0 Kudos
Reply
0 Replies