IMXRT10** DCDC_OUT accuracy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMXRT10** DCDC_OUT accuracy

跳至解决方案
1,075 次查看
gavin5342
Contributor III

I can't see the accuracy spec for the DCDC converter on IMXRT10**.  The reason for asking is that the datasheet specifies, for VDD_SOC min 1.15V for normal operation and 1.25V for overdrive.

I have seen some SDK examples set DCDC_OUT to 1.25V for overdrive configuration and others set DCDC_OUT to 1.275V for overdrive.

0 项奖励
回复
1 解答
995 次查看
lucas_cao
NXP Employee
NXP Employee

1.275V is the correct voltage, the 1.25V setting in SDK code should be updated.

在原帖中查看解决方案

4 回复数
996 次查看
lucas_cao
NXP Employee
NXP Employee

1.275V is the correct voltage, the 1.25V setting in SDK code should be updated.

990 次查看
gavin5342
Contributor III

Thanks very much! That makes most sense to me too.

0 项奖励
回复
997 次查看
gavin5342
Contributor III

I am interested in the answer for RT1050 series and RT1010 series.  For both of these devices the range is 1.15 - 1.3V as you show here.

0 项奖励
回复
1,063 次查看
diego_charles
NXP TechSupport
NXP TechSupport

Hi @gavin5342 

I hope you are doing great! 

To give you a better response :  could you specify in which part number and related SDK did you saw those parameters and  DCDC output settings?

For example, according to the RT1060 DS, the VDD_SOC_IN tolerates up to 1.3v

diego_charles_0-1693590548139.png

All the best, 

Diego

 

0 项奖励
回复