IMX RT1061 custom board is not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX RT1061 custom board is not working

跳至解决方案
1,307 次查看
ThomasSC
Contributor III

Hi,

unfortunately, our first custom board with a member of the i.MX RT family does not work. We have a 24 MHz crystall at the oscillator pins.

At the oscillator output XTALO is only a DC signal with about 1.11 V and no oscillation.

What can be the cause and needs to be checked?

Thanks & Regards,

Thomas

0 项奖励
回复
1 解答
1,271 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer RT1060 hardware design guide, the Table 4 provide some guideline about 24MHz oscillator circuit design. 

The voltage should be ok: The logic level of this forcing clock must not exceed the NVCC_PLL (1.1V) level.

Load capacitor must chosse properly to align with crystal spec specified.

Bias XTALI with a 2.2 M resistor to GND.

Mount the resistor close to the XTALI ball.

Wish it helps.

Mike

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,272 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer RT1060 hardware design guide, the Table 4 provide some guideline about 24MHz oscillator circuit design. 

The voltage should be ok: The logic level of this forcing clock must not exceed the NVCC_PLL (1.1V) level.

Load capacitor must chosse properly to align with crystal spec specified.

Bias XTALI with a 2.2 M resistor to GND.

Mount the resistor close to the XTALI ball.

Wish it helps.

Mike

0 项奖励
回复
1,256 次查看
ThomasSC
Contributor III

Hi,

now the oscillator runs after placing a 4.7uF capacitor at VDD_SNVS_CAP.

Thanks

Thomas

0 项奖励
回复