Can i.MX RT1176 work with eMMC version 5.1 and up?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i.MX RT1176 work with eMMC version 5.1 and up?

Jump to solution
279 Views
puiyee_poon
Contributor I

Hi NXP team,

In the datasheet, the MCU i.MX RT1176 supports MMC up to version 5.0. 
However, it is easier to find memories with versions 5.1 and upwards. 
My question is: Will the MCU function with memories supporting versions 5.1 and upwards but the MCU will not support the functionalities for versions 5.1 and upwards?

Br // PuiYee

0 Kudos
Reply
1 Solution
266 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @puiyee_poon ,

    I have purchased one samsung emmc 5.1 previously, and I have tested it on the RT1176, no matter the directly communication or the code boot from emmc, it works OK.

  So, at least the emmc5.1 works, to the up version, you may need to test it on your side.

Wish it helps you!

Best Regards,

Kerry

View solution in original post

0 Kudos
Reply
1 Reply
267 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @puiyee_poon ,

    I have purchased one samsung emmc 5.1 previously, and I have tested it on the RT1176, no matter the directly communication or the code boot from emmc, it works OK.

  So, at least the emmc5.1 works, to the up version, you may need to test it on your side.

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply