CAN peripheral is not working properly in cm7 while using dual core in IMXRT1175 controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN peripheral is not working properly in cm7 while using dual core in IMXRT1175 controller

564 Views
arvind2
Contributor I

Hello!

          I am facing an issue while using CAN in dual core after  "power on" CAN is not working in cm7 of IMXRT1175 controller.( #i.MXRT1175 ) #CAN #dual_core #cm7

when we are using individual cores CAN is working after power on .And also CAN is working fine in cm4 in dual core after power on but it's not working in cm7 dual core mode after "power on". Please provide the solution for this issue.

yours sincerely

ARAVIND.

 

 

0 Kudos
Reply
1 Reply

518 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @arvind2,

Could you please help us with more information?

Are you using an NXP EVK board, or is it a custom one? Could you give us details of your code, for example, a snippet showing how you initialized and configured the dual core and CAN functionalities? Are you using CAN FD or FlexCAN drivers? Which examples are you using or could be used to replicate your issue?

Best regards, Raul. 

0 Kudos
Reply