About the problem of sector erasing in 【driver_examples\flexspi\nor\polling_transfer】 routines

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the problem of sector erasing in 【driver_examples\flexspi\nor\polling_transfer】 routines

773 Views
fancyop
Contributor I

driver_examples\flexspi\nor\polling_transfer 

There is no write enablement in the flexspi_nor_flash_erase_sector program,The original program is:

pastedImage_1.png

It should be written as the following program, the section in the red box needs to be addedotherwise the erase sector will not succeed.

pastedImage_2.png

Labels (1)
0 Kudos
Reply
2 Replies

678 Views
jeremyzhou
NXP Employee
NXP Employee

Hi  Op Fancy

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Thanks for your reply, I'd like to do a test by myself to replicate the phenomenon you mentioned, so whether you can tell me which RT chip you talk about.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

678 Views
fancyop
Contributor I

i.MX RT1050

pastedImage_1.png

0 Kudos
Reply