About Using 12bit address SDRAM on RT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About Using 12bit address SDRAM on RT1170

257 Views
dskim2
Contributor III

Hi

I am testing the RT1170 custom board with 12bit address 16MB SDRam, but it is not working properly.
There is only one 16MB SDRam connected to the board.

The RT1170 EVK board is equipped with 13 bit 64MB SDRam, so I need to modify the sample source. How can I do that?

Also, how should I connect the HW?
EVK has two 32MB SDRams, but the custom board has only one 16MB SDRam.

Please refer to the attached source and applied SDRAM data sheet.

Best Regards

Tags (1)
0 Kudos
Reply
1 Reply

210 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @dskim2 ,

 

I don't think the connection needs to be changed, you may just copy the connection from EVK, but the MPU settings should be modified according to the new SDRAM size. Please refer to board.c for more details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply