1060 evk12 cannot debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1060 evk12 cannot debug

791 次查看
jingyangxie
Contributor V

I have a board(imxrt1060-evk12) ,when i use the sdk2.12.1 for 1060-evk, it cannot debug with flexspi_nor link file:

jingyangxie_0-1670216875899.jpeg

 

0 项奖励
5 回复数

751 次查看
lucas_cao
NXP Employee
NXP Employee

Hi @Alice_Yang  and @jingyangxie 

RT1060 EVK12 used HyperFlash as the boot device. 

So if you are using RT1060's SDK, it makes sense that it cannot work well.

You can try RT1050 SDK becasue it uses HyperFlash as the boot device.

BTW, where did you get the RT1060 EVK12 board? By university program?

 

 

781 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jingyangxie 

It seems there is an issue with the boot jumper:

Alice_Yang_0-1670403158761.png

 

Have a look at :

https://www.nxp.com/document/guide/get-started-with-the-mimxrt1060-evk:GS-MIMXRT1060-EVK  

 

BR

Alice

0 项奖励

764 次查看
jingyangxie
Contributor V

I have changed the SW7 to 0010, but it still doesn't work.the log as follows

0 项奖励

757 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jingyangxie 

Which demo do you run? How about iled_blinky under SDK?

 

BR

Alice

0 项奖励

755 次查看
jingyangxie
Contributor V

it can not work too if I use the flexspi_nor.icf link file

0 项奖励