wm8960声卡驱动移植

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

wm8960声卡驱动移植

2,708 次查看
韩士龙
Contributor I

请问大神:怎么移植wm8960声卡驱动到imx6q上呢?能否把wm8960驱动源码和移植步骤给一份呢?谢谢了!

标签 (1)
标记 (1)
0 项奖励
4 回复数

1,438 次查看
leige-b42127
Senior Contributor II

你能和FAE申请到我们公司来吗?你带设备来,我帮你一起调。

0 项奖励

1,438 次查看
韩士龙
Contributor I

您好:

太远了,您只要把wm8960的源码和移植步骤给我就行了,谢谢!

2015-01-16

石家庄开发区天远科技有限公司

开发一部 韩士龙

手机:15127185610

地址:石家庄市黄河大道227号

发件人:Lei Ge <admin@community.freescale.com>

发送时间:2015-01-16 11:12

主题:Re: - wm8960声卡驱动移植

收件人:"士龙 韩"<hanshilong622@163.com>

抄送:

wm8960声卡驱动移植

reply from Lei Ge in i.MX Community - View the full discussion

你能和FAE申请到我们公司来吗?你带设备来,我帮你一起调。

Did your question get answered?

If so, say thanks by clicking Correct Answer in the community thread!

Reply to this message by replying to this email, or go to the message on Freescale Community

Start a new discussion in i.MX Community by email or at Freescale Community

Following wm8960声卡驱动移植 in these streams: Inbox

0 项奖励

1,438 次查看
谢骆冰谢
Contributor I

士龙兄,能否把源码给我来一份?我的工作也卡在这了,邮箱:767923274@qq.com,在此先谢过!

0 项奖励

1,438 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 士龙

one can use WM8962 codec driver, since WM8962 is used on Sabre board

i.MX6_SABRE_SDP_DESIGNFILES : Design files (SPF-27392 p.10)

attached Linux Manual Table 23-1. Stereo Codec SoC Driver Files

shows driver files location

L3.0.35_4.1.0_ER_SOURCE_BSP : i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite,

i.MX 6Solo and i.MX 6Sololite Linux BSP Source Code Files

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励