will imx25 support ext3 filesystem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

will imx25 support ext3 filesystem

797件の閲覧回数
gurumoorthirasi
Contributor IV

Dear All,

I am using linux 2.6.31 kernel with freescale BSP downloaded from freescale imx25 product page only.

will that officially released kernel 2.6.31 support ext3 file system ? .

if not what I need to do to change file system to ext3.

as of now as per official document i am using ext2 file system.

Regards,

Guru

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 返信

645件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi guru

yes it supports it, please refer to p.27 attached document:

8.Format the MMC/SD partitions as ext3 type

root@freescale ~$ mkfs.ext3 /dev/mmcblk0p1

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信