why does the cvbs video of IMX6SOLO shake,capture from isl79987?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

why does the cvbs video of IMX6SOLO shake,capture from isl79987?

604件の閲覧回数
翔李
Contributor IV

4ch camera CVBS video captyre to isl79987,then outputs mipi to imx6 solo,and outputs cvbs by adv7391 to monitor,but the cvbs video shakes like water,refer to video of attachment.

pastedImage_1.png

pastedImage_2.png

2 返答(返信)

390件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

one can test if this is caused by high processor loading: decrease

camera fps and resolution. Remove from image other applications and

disable cpufreq and bus frequency drivers, pleasee refer to attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

390件の閲覧回数
翔李
Contributor IV

Thanks.

Is there a demo board on imx6solo be good for isl79987 mipi video capture?I know that imx6q works well with isl79987.

0 件の賞賛