what are the configuration in dts file(4.1.15_1.2.0_ga) should follow for wifi and bluetooth while flashing through sd card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what are the configuration in dts file(4.1.15_1.2.0_ga) should follow for wifi and bluetooth while flashing through sd card

4,515 Views
kishore_k
Contributor I

how to enble the wifi and bluetooth in imx6ul board when flash through sd card. While i am enabling the wifi bluteooth in dts i am getting kernel panic.

root@imx6ulnxpuiopb:~# ifconfig -a
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00 
NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10 
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:25

eth0 Link encap:Ethernet HWaddr CE:57:FB:EA:B1:6A 
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000 
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

lo Link encap:Local Loopback 
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:12 errors:0 dropped:0 overruns:0 frame:0
TX packets:12 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0 
RX bytes:800 (800.0 B) TX bytes:800 (800.0 B)

sit0 Link encap:IPv6-in-IPv4 
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0 
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)

Labels (1)
0 Kudos
Reply
1 Reply

3,796 Views
romitchatterjee
Contributor V

Which Wi-Fi/BT module are you using, and how have you connected it to the board?

0 Kudos
Reply