waylandsink's fullscreen property is causing an error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

waylandsink's fullscreen property is causing an error

1,957 Views
itaigolan
Contributor II

Hello,

I'm using an imx8mp on a variscite dart board. I want to make my application take up the entire screen. To achieve this I tried running the following pipeline:

gst-launch-1.0 -v videotestsrc ! waylandsink fullscreen=true

But I got the following error:

ERROR: from element /GstPipeline:pipeline0/GstWaylandSink:waylandsink0: Window has no size set
Additional debug info:
/usr/src/debug/gstreamer1.0-plugins-bad/1.20.3.imx-r0/ext/wayland/gstwaylandsink.c(1143): gst_wayland_sink_show_frame (): /GstPipeline:pipeline0/GstWaylandSink:waylandsink0:
Make sure you set the size after calling set_window_handle
ERROR: pipeline doesn't want to preroll.
Setting pipeline to NULL ...
ERROR: from element /GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0: Internal data stream error.
Additional debug info:
/usr/src/debug/gstreamer1.0/1.20.3.imx-r0/libs/gst/base/gstbasesrc.c(3127): gst_base_src_loop (): /GstPipeline:pipeline0/GstVideoTestSrc:videotestsrc0:
streaming stopped, reason error (-5)
ERROR: pipeline doesn't want to preroll.
Freeing pipeline ...

I also looked at setting the size after set_window_handle is called as is mentioned in the error log but I couldn't figure out how to do that. Does anyone know how I might go about solving this problem?

Labels (1)
0 Kudos
Reply
1 Reply

1,932 Views
pierluigi_p
Senior Contributor I

Hi @itaigolan,

to disable the weston panel, you may want to edit the file

 

/etc/xdg/weston.ini

 

and add / modify the dedicated shell section with

 

[shell]
panel-position=none

 

Be aware that wayland plugin introduces a fixed PANEL_HEIGHT of 32 pixels which is used to decrease the full-screen height.

You may want to hack the plugin to customize this behavior according your needs.

Best Regards

Pier

0 Kudos
Reply