v7_dma_clean_range+0x20

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

v7_dma_clean_range+0x20

1,055 Views
aoboyan
Contributor I


Ipsec (openswan) secure channel is transplanted in imx6ull chip  on kernal 4.3..., but the following error will be prompted, please tell me how to solve it. This should be a platform issue. I have seen other people raise this issue in the community, but I have not found a solution.

  •  INFO: IPsec-SA established: ESP/Tunnel 192.168.3.77[500]->192.168.3.1[500] spi=7872688)
    DEBUG: ===


    Unable to handle kernel paging request at virtual address 70000000
    pgd = 80004000
    [70000000] *pgd=00000000
    Internal error: Oops: 805 [#1] PREEMPT SMP ARM
    Modules linked in: esp4 xfrm4_mode_tunnel hmac ov5642_camera mxc_v4l2_capture ipu_bg_overlay_sdc ipu_still g
    CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.1.15-1.1.1+gd5d7c02 #1
    Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree)
    task: 80b038f0 ti: 80afe000 task.ti: 80afe000
    PC is at v7_dma_clean_range+0x20/0x38
    LR is at __dma_page_cpu_to_dev+0x28/0x94
    pc : [<8001ee3c>] lr : [<8001ad90>] psr: 000f0113
    sp : 80affc48 ip : ab757000 fp : 00000000
    r10: a89e8b40 r9 : a876b410 r8 : 00000000
    r7 : 00000001 r6 : 00000000 r5 : ab557000 r4 : 00000000
    r3 : 0000001f r2 : 00000020 r1 : 70000000 r0 : 70000000
    Flags: nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
    Control: 10c53c7d Table: 389b004a DAC: 00000015
    Process swapper/0 (pid: 0, stack limit = 0x80afe210)
    Stack: (0x80affc48 to 0x80b00000)

    ......

Labels (1)
0 Kudos
Reply
1 Reply

986 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Try enable new kernel on it, I saw this problem before and I think the 4.14.98 solve this issue. But You want to use the MX6ULL and the boot said the MX6QD device tree, I think there is change in DDR and 1GB and 512MB please check it.

Regards

0 Kudos
Reply