u-boot stuck for imx8QM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

u-boot stuck for imx8QM

573 次查看
brijesh9
Contributor I

u-boot 2021.04 working fine but u-boot 2023.04 version stuck for imx8qm (attached both pic)

using latest version of yocto for create u-boot

i'm using below command for config 

make imx8qm_mek_defconfig

 

U-Boot 2023.04-70991-g75c2df1f1f (Jan 24 2024 - 11:37:03 +0530)

CPU: NXP i.MX8QXP RevA A53 at 0 MHz at 25C

Model: NXP i.MX8QM MEK
Board: iMX8QM MEK
Boot: MMC0
DRAM: 2 GiB
imx_lpi2c i2c@5a800000: Failed to get i2c clk: 0
imx_lpi2c i2c@5a800000: Failed to get i2c clk: 0
setup_typec: tcpc init failed, err=-62
Core: 188 devices, 32 uclasses, devicetree: separate
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... esdhc_set_voltage error -11
esdhc_set_voltage error -11
esdhc_set_voltage error -11
*** Warning - bad CRC, using default environment

[*]-Video Link 0imx_lpi2c i2c@56247000: Failed to get i2c clk: 0
imx_lpi2c i2c@56247000: Failed to get i2c clk: 0

<-------------- STUCK HERE

0 项奖励
回复
0 回复数