u-boot stopped at -Video Link 0 while booting mx8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

u-boot stopped at -Video Link 0 while booting mx8

491 次查看
brijesh9
Contributor I

u-boot stopped at -Video Link 0 while booting mx8

followed below Document

https://variwiki.com/index.php?title=Yocto_Build_U-Boot&release=mx8-yocto-mickledore-6.1.22_2.0.0-v1...

below are the message print on terminal while booterror_u-boot.PNG

 

 

U-Boot 2023.04-70991-g75c2df1f1f (Jan 18 2024 - 00:09:59 +0530)

CPU: NXP i.MX8QXP RevA A53 at 0 MHz at 25C

Model: Variscite VAR-SOM-MX8
Boot: MMC0
DRAM: 2 GiB
imx_lpi2c i2c@5a810000: Failed to get i2c clk: 0
imx_lpi2c i2c@5a810000: Failed to get i2c clk: 0
pca953x gpio@20: Error reading output register
pca953x gpio@20: Error reading output register
pca953x gpio@20: Error reading output register
Core: 182 devices, 28 uclasses, devicetree: fit
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... esdhc_set_voltage error -11
esdhc_set_voltage error -11
esdhc_set_voltage error -11
*** Warning - bad CRC, using default environment

[*]-Video Link 0

0 项奖励
回复
4 回复数

430 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Suggest to get help from variscite.

 

Regards

Harvey

0 项奖励
回复

403 次查看
brijesh9
Contributor I

hi i'm using imx 8 processor.

https://github.com/nxp-imx/uboot-imx

above u-boot i'm using, its working for 2021 version bet not working for 2023 version

0 项奖励
回复

447 次查看
brijesh9
Contributor I

i'm using it for Virtual Environment QEMU

0 项奖励
回复

447 次查看
brijesh9
Contributor I

it is working fine with 2021 u-boot version but failing 2023(i want to use latest version 2023)

working_u_boot.PNG

0 项奖励
回复