sch of IMXQ6Q compatibity with IMX6DUAL-LITE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sch of IMXQ6Q compatibity with IMX6DUAL-LITE

247 Views
翔李
Contributor IV

hi,

  I alreday design sch. of IMX6Q(MCIMX6Q5EYM10AD),now I need to let sch of IMXQ6Q compatibity with IMX6DUAL-LITE(MCIMX6U5EVM10AC).It means that I can solder IC IMX6Q or IMX6DUAL-LITE on the same PCB board.

  what is the detailed difference between IMX6Q and IMX6DUAL-LITE ON sch? Give me the doc

or sch-demo,thanks.

Labels (3)
0 Kudos
1 Reply

201 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to AN4397 : “Common Hardware Design for i.MX 6Dual/6Quad
and i.MX 6Solo/6DualLite”

http://cache.nxp.com/files/32bit/doc/app_note/AN4397.pdf

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos