sc_seco_authenticate doesn't return error but seco events shows AHAB_NO_AUTHENTICATION_IND

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sc_seco_authenticate doesn't return error but seco events shows AHAB_NO_AUTHENTICATION_IND

1,100 Views
bulat_a
Contributor III

Hi all,

Noticed that the following commands in uboot are always successful even the container image was no signed, but "seco events" shows that the image was not signed (AHAB_NO_AUTHENTICATION_IND):

Uboot>if run auth_os; then echo Done; else echo ERR; fi; - it almost the same what uboot will do if we enable:

#define AHAB_ENV "sec_boot=yes\0"
 

So, I enabled CONFIG_AHAB_BOOT to use SECO API from uboot

generated keys and signed containers follow to AHAB guides and burned SRK_HASH fuses.

1th container image  - signed flash.bin with SCU, uboot, SCFW that works fine. No SECO events

2th container image -  flash_os.bin (Linux Kernel + DTB)  unsigned and

                                     flash_os.bin.signed with the same keys as a previous one and it should be authenticated by uboot via SECO API

 

So, if you look at the screenshot:

run auth_os-> auth_cntr -> do_authenticate -> authenticate_os_container -> sc_seco_authenticate  -< No errors

But "seco events" shows(or not shows the errors depending on Linux image) AHAB_NO_AUTHENTICATION_IND

Thus, the questions are:

  • Is it related to the fact that the device in "NXP Closed" state? 
  • Will the "sc_seco_authenticate" return the error when the device will be closed or does it just say that command passed and we should check the result with ahab_status?

 

Regards,

Bulat

0 Kudos
Reply
1 Reply

1,095 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

You can see at the end of apply_snvs_config function, the hp.lock(0x1f0703ff) and lp.lock(0x1f0003ff) will be set, so the LPTGFCR_HL and LPTGFCR_SL will both set to 1.

The 0x44 SNVS register is SNVS_LPSM_LP Tamper Glitch Filters Configuration Register, which is used to configure the glitch filters for the SNVS_LP tamper inputs. This register cannot be programmed when
the LPTGFCR_SL or LPTGFCR_HL bit is set. 

Meanwhile, from below description, you can know the reset conditions of these two bits. Cold reset will make these two bits reset, warm reset can't, so the failure appeared. 

SNVS_LP Lock Register

b45499_0-1631759552604.png

 

SNVS_HP Lock Register

b45499_1-1631759552342.png

 

0 Kudos
Reply