reset key can't reboot system

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

reset key can't reboot system

667 Views
yan2anfei
Contributor III

hi ,

I have a custom board base on imx6sl, 

when the system is booting  , press reset button,system can reboot, but if the system boot complete,press reset button, the system do anything,Looks like  crash. 

Has some people encountered this situation and how to solve?

thanks.

Labels (2)
0 Kudos
1 Reply

513 Views
igorpadykov
NXP Employee
NXP Employee

Hi yan2

please refer to attached Release Notes

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos