"No GSettings schemes are installed on the system" error when running gnome-bluetooth on i.MX6Q SABRE SD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"No GSettings schemes are installed on the system" error when running gnome-bluetooth on i.MX6Q SABRE SD

1,567 Views
alvind
Contributor III

Hello everyone,

I bitbaked the recipe "gnome-bluetooth", which produced four binaries, namely bluetooth-applet, bluetooth-properties, bluetooth-wizard, and bluetooth-sendto. I transferred the contents of the gnome-bluetooth's "image" folder into their corresponding folder hierarchy in the target filesystem, so that the shared libraries and other related files are in their proper folder in the target. Now when I tried running the "bluetooth-applet" binary, the following error appeared:

"GLib-GIO-ERROR: No GSettings schemes are installed on the system. Trace/breakpoint trap"

The same error also appeared when I tried to run bluetooth-properties. Strangely enough, the remaining two binaries bluetooth-sendto and bluetooth-wizard can start. I was wondering if anyone has used the gnome-bluetooth manager for their board, and if anyone also encountered the same error. I know I did a mistake somewhere in the process, but I would appreciate if anyone can point me in the right direction. BTW,  my host platform is an x86 64 bit PC with Ubuntu 12.04 LTS.

Thank you!

Labels (3)
3 Replies

952 Views
alvind
Contributor III

Hello,

I want to update this thread since I managed to make some progress, but now I am encountering a different problem. Here's what I did:

1) I added gnome-bluetooth and gsettings-desktop-schemas to the fsl-image-x11 recipe and bitbaked fsl-image-x11

2) After SABRE booted up I entered "export DISPLAY=:0.0"

3) I tried to start the "bluetooth-applet", but after entering the command bluetooth-applet, I was greeted by this error: "org.gnome.Bluetooth schema not installed". So I searched around the target filesystem and found out .xml files including the one for gnome-bluetooth, and learned that I needed to install these .xml files from this link: https://developer.gnome.org/gio/stable/ch32s06.html. Basically I needed to run this command "glib-compile-schemas </usr/share/path to xml schemas>".

4) After compiling the GSettings schema for gnome-bluetooth, I tried running "bluetooth-applet" from the command line and now this error shows up: "GLib-GIO Message: Using the 'memory' GSettings backend. Your settings will not be saved or shared with other applications." Nothing shows up but whenever I run the "configure bluetooth" app on the Yocto Project desktop, a window appears successfully. I can also run the other three binaries from the command line.

Whenever I reboot the board I need to run steps 2 and 3 first before I can run the gnome-bluetooth binaries. I'll post updates once I make progress on this problem.

952 Views
gusarambula
NXP TechSupport
NXP TechSupport

Thanks for posting your progress! There is indeed nor much information on this feature. Even the Gnome Help is a bit short on documentation on their Schemas.

Please keep us posted on your progress!

952 Views
alvind
Contributor III

Thanks gusarambula,

I got rid of the "GSettings memory backend" message by adding the package "dconf" to the fsl-image-x11 recipe. From my understanding GSettings and Dconf work together: Gconf, Dconf, Gsettings and the relationship between them - Ask Ubuntu. Now I only need to find out how to install the .xml file automatically at startup, without typing "glib-compile-schemas </path to xml schemas>" always. Also, I now need to test if gnome-bluetooth can actually pair devices via Bluetooth, which is an altogether different problem :smileyhappy:

0 Kudos