mx6q can support dual usb uvc camera in android 4.3 system?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mx6q can support dual usb uvc camera in android 4.3 system?

Jump to solution
1,261 Views
mrleo
Contributor IV

Hi all,

    My custom board is mx6q board,I want support two usb uvc camera.

    One is ok for me,please help me how to support two usb uvc camera?

    Can it open at the same time?

Thanks,

Leo

0 Kudos
1 Solution
803 Views
mrleo
Contributor IV

Hi Victor Linnik,

So two usb camera can't support in android.But can support in linux system.

Thanks Very much!

View solution in original post

0 Kudos
2 Replies
804 Views
mrleo
Contributor IV

Hi Victor Linnik,

So two usb camera can't support in android.But can support in linux system.

Thanks Very much!

0 Kudos
803 Views
b36401
NXP Employee
NXP Employee

You can connect 2 USB cameras to i.MX6 fine.

Please refer "Using a USB Camera with GStreamer" document

https://community.freescale.com/docs/DOC-93688

regarding connecting the cameras.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos