Hi,
I want to use sn65dsi84 to display single dsi as dual lvds on my custom board.
My development environment is imx8qxp in linux kernel 5.15.71.
The problem is that no mipi-dsi signal on board.
I referred to the settings from the imx8qxp-mek.dts file.
This is configuration of my dts.
-------------------------------
&mipi1_dphy {
status = "okay";
};
Please refer below rules.
1.Define sn65dsi84 in i2c node
bridge@2c {
compatible = "ti,sn65dsi84";
reg = <0x2c>;
enable-gpios = <&gpiof 15 GPIO_ACTIVE_HIGH>;
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
bridge_in: endpoint {
remote-endpoint = <&dsi_out>;
data-lanes = <1 2>;
};
};
port@2 {
reg = <2>;
bridge_out: endpoint {
remote-endpoint = <&panel_in_lvds>;
};
};
};
};
2. Define panel-lvds in root node , not mipi dsi node
panel@0 {
compatible = "panel-lvds";
/* Physical dimensions of active area */
width-mm = <338>;
height-mm = <270>;
data-mapping = "vesa-24";
panel-timing {
/* the hactive and porches in the datasheet are for a single LVDS channel */
/* since we use dual LVDS channel, Horizontal paramter and clock must double*/
clock-frequency = <41238000>;
hactive = <640>;
hsync-len = <10>;
hfront-porch = <70>;
hback-porch = <70>;
vactive = <1024>;
vsync-len = <10>;
vfront-porch = <5>;
vback-porch = <5>;
};
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
dual-lvds-odd-pixels;
panel_in_a: endpoint {
remote-endpoint = <&bridge_out_a>;
};
};
port@1 {
reg = <1>;
dual-lvds-even-pixels;
panel_in_b: endpoint {
remote-endpoint = <&bridge_out_b>;
};
};
};
};
port {
dsi_out_port: endpoint {
remote-endpoint = <&bridge_in>;
data-lanes = <0 1 2 3>;
};
};
};
3.Define mipi dsi out node in mipi1_dsi_host
&mipi1_dsi_host {
status = "okay";
ports {
port@1 {
reg = <1>;
mipi1_adv_out: endpoint {
remote-endpoint = <&adv7535_1_in>;
};
};
};
};
Thanks for your reply.
I tried running it after making some modifications, but it's not working properly.
Error running "drm_of_find_panel_or_bridge" function on "ti-sn65dsi83.c".
More specifically, it happened in the "of_drm_find_panel".
I think it's because of the incorrect kernel configuration.
So could you please check the attached config file(config.txt) and let me know what needs to be revised?
Thanks for the reply.
Following your guide, there are no more errors.
However, it still doesn't work.
When I checked the dsi line with the oscilloscope, I couldn't see the signal.
Is there anything else I can look at about why the dsi signal is not transmitting?
And below is current drm list.
Also refer to the attached dts file(sn65dsi84.dts), panel-simple.c and kernel config(config.txt).
----------------------------
root@:~# ls -l /sys/class/drm/
total 0
lrwxrwxrwx 1 root root 0 Apr 28 17:42 card0 -> ../../devices/platform/display-subsystem/drm/card0
lrwxrwxrwx 1 root root 0 Apr 28 17:42 renderD128 -> ../../devices/platform/display-subsystem/drm/renderD128
-r--r--r-- 1 root root 4096 Apr 28 17:42 version
root@:~# ls -l /sys/class/drm/card0/
dev device/ power/ subsystem/ uevent
root@:~# ls -l /sys/class/drm/card0/
total 0
-r--r--r-- 1 root root 4096 May 5 09:56 dev
lrwxrwxrwx 1 root root 0 May 5 09:56 device -> ../../../display-subsystem
drwxr-xr-x 2 root root 0 May 5 09:56 power
lrwxrwxrwx 1 root root 0 Apr 28 17:42 subsystem -> ../../../../../class/drm
-rw-r--r-- 1 root root 4096 Apr 28 17:42 uevent
Please use one typical timing for test and provide kernel log.
Can you add more log print in sn65dsi83 driver and enable debug flag in drivers/gpu/drm/bridge/nwl-dsi.c ? Please check MIPI HOST driver status.
Thanks for your reply.
I tried to enable debug flag in nwl-dsi.c like below, but it doesn't show debug message.
So could you please let me know how to enable debug flag in driver?
The log should contain 'imx-drm display-subsystem', need check dts nodes.
[ 3.155378] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.163871] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.171546] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.179325] imx-drm display-subsystem: bound bus@56220000:ldb@562210e0 (ops imx8qxp_ldb_ops)
[ 3.187908] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /bus@56220000/dsi_host@56228000 to encoder DSI-89: -19
[ 3.199019] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component_ops)
[ 3.207751] imx-drm display-subsystem: bound bus@56220000:ldb@562410e0 (ops imx8qxp_ldb_ops)
[ 3.216240] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /bus@56220000/dsi_host@56248000 to encoder DSI-89: -19
[ 3.227335] imx-drm display-subsystem: bound 56248000.dsi_host (ops nwl_dsi_component_ops)
[ 3.236054] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
Please include evk dts in your dts or add dc/dpu node like mek.dts
Thanks for your reply.
Referring to imx8qxp-ss-lvds.dtsi and imx8qxp-ss-dc.dtsi, I tried to activate 'imx-drm display-subsystem' in 2 ways, but it is failed.
The first way is to add 'display-subsystem' in existing dts.
Please refer to the attached subsystem.dts.
In this case, 'imx-drm display-subsystem' log is not displayed.
The second way is to use dpu, refer to the attached 'dpu_subsystem.dts'.
This causes kernel panic.
I am not familiar with it.
So would you please let me know how to enable 'display-subsystem'.
Are you using linux-imx? You can modify imx8qxp-mek.dts and add this video bridge based on ADV7535. Then you don't need modify any driver config and device tree node.
Thanks to your reply.
As you said, I use linux-imx.
However, base image is different from imx8qxp-mek.dts.
Even I tried to reference the imx8qxp-mek image as much as possible, but display-subsystem log is not displayed.
I think due to a slight difference, my board doesn't work.
Anyway, thanks to your help, it is very helpful to me.