mfgtool burn imx8mq evk fails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mfgtool burn imx8mq evk fails

694 次查看
chhsu0229
Contributor II

I am working on burning Linux OS on om8mq evk SD card and it is failed. My steps are following,

1. SW801 is '0010' and SW is '01

2. double click L4.9.88_2.0.0_mfg-tool_MX8MQ\mfgtools-with-rootfs-mx8\mfgtools\mfgtool2-yocto-mx8-evk-sd2.vbs

3. MfgTool shows

1.JPG

I confirmed that there are files in the Profiles/Linux/OS Firmware/files

 

How can I fix this issue?

Thanks

0 项奖励
回复
1 回复

676 次查看
nxf63675
NXP TechSupport
NXP TechSupport

Hi chhsu0229,

 

It appears that the tool did not found the u-boot file, could you check to the debug window and attach the result? Also attach the mfgtool.log to see if there is something more I am missing, In any case, verify that you have the u-boot and .sdcard files.

 

Regards,

Israel.

0 项奖励
回复