load capacity for SD pin of i.MX6Solo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

load capacity for SD pin of i.MX6Solo

426 Views
yuuki
Senior Contributor II

Dear all,

We want to evaluate the AC timing of the SD card.
Would you tell me the terminal load capacity about each pin?
(tolerance and dispersion(Variation) by the temperature)

I referred to a data sheet, but was not able to find it.

Best Regards,
Yuuki

Labels (1)
0 Kudos
1 Reply

350 Views
Yuri
NXP Employee
NXP Employee

Hello,

You may use device IBIS model to get such pins parameter as capacity.

https://www.nxp.com/webapp/Download?colCode=IMX6_DL_S_IBIS&appType=license&Parent_nodeId=13376968519... 

i.MX6S|i.MX 6Solo Processors|Multimedia|NXP 

C_pkg typ = 7.39741pF
C_pin of SD1_DATA0  is 1.29006pF

  Let me remind, if R_pin, L_pin, and C_pin parameters (FOR THAT PIN ONLY) are
not declared, this means the default package values (R_pkg, L_pkg, C_pkg,
specified under [Package]) should be used.
And, if individual pin parasitic value of R_pin, L_pin and C_pin are available,
the values R_pkg, L_pkg and C_pkg are ignored. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos