libmcc for imx6 solox

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

libmcc for imx6 solox

1,390 Views
troide
Contributor II

Hello community,

Is there any tested libmcc available for imx6sx. I tried the driver in the original package but it seems it has some issues. any alternative?

Cheers,

Sina

Labels (1)
0 Kudos
Reply
3 Replies

1,064 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sina

latest 3.14.52 BSP includes RPMsg driver, description can be found

in attached Linux Manual Chapter 52.

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

I am not aware of other mcc libraries.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,064 Views
troide
Contributor II

Hello Igor,

Thanks for the quick replay. Actually we are aware of the RPMsg driver but the point is that we couldn't find any proper RTOS image is used for the Cortex-M4 processor. In the document it is mentioned that the Cortex-M4 processor RTOS should run on the QSPI NOR flash on the i.MX 6SoloX. Is there any RTOS image avaible that we can download for this purpose? Is the driver avaiable on the RTOS side?

Cheers,

Sina

0 Kudos
Reply

1,064 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sina

i.MX 6SoloX uses MQX

MQX™ Software Solutions|NXP

Best regards

igor

0 Kudos
Reply