lcd和hdmi显示yuv格式的数据的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lcd和hdmi显示yuv格式的数据的问题

1,871 Views
yyuan
Contributor III

 

lcd和hdmi显示yuv格式的数据的问题

大家好    板子型号是imx6q    核是4.1.15   

bootargs  :  setenv displayinfo 'video=mxcfb0:dev=lcd,MDP02BP,if=VYUY16

video=mxcfb1:dev=hdmi,1920x1080M@60,if=VYUY16'
或者

setenv displayinfo 'video=mxcfb0:dev=lcd,MDP02BP,if=VYUY16

video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24'



lcd输出为yuv422的数据    

我们理解的是hdmi的数据不会受到lcd的数据格式的影响,所以开始想hdmi的数据为rgb的就可以,但是lcd上的图像是正常的,但是hdmi的图像不正常   图像是绿色的

请问是什么情况呢   需要对hdmi的驱动进行修改吗?

谢谢

0 Kudos
3 Replies

1,546 Views
joanxie
NXP TechSupport
NXP TechSupport

if HDMI+LCD,you can refer to the command as below I have tested successfully:
video=mxcfb0:dev=lcd,SEIKO-WVGA,if=RGB24 bpp=32
video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24 bpp=32

0 Kudos

1,546 Views
yyuan
Contributor III

thank you

i need to set yuv output .   i test  , RGB output  is ok.

now   i need yuv output. 

please can you help me again?

thank you again.

0 Kudos

1,546 Views
joanxie
NXP TechSupport
NXP TechSupport

I have replied to you in chinese community, any update, you can reply there in chinese

0 Kudos