Hello,
I am adding iptables to an image built with https://github.com/Freescale/fsl-community-bsp-platform/tree/rocko.
To modify the kernel config I use "bitbake -c menuconfig linux-imx" and enable the required netfilter modules, I also added iptables and kernel-modules in my local.conf file:
PACKAGE_CLASSES ?= "package_ipk"
CORE_IMAGE_EXTRA_INSTALL += " kernel-modules"
IMAGE_INSTALL += " \
kernel-modules \
iptables
"
The kernel modules for netfilter are not added to the rootfs and the packages are not generated in tmp/deploy/ipk
The kernel version is 4.9.11.
Seems related to: https://community.nxp.com/t5/i-MX-Processors/ip-tables-does-not-get-included-in-kernel-modules/td-p/...
Could be related to the rocko version of fsl-community-bsp-platform?.
Thanks for your help.