imx8qm jailhouse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm jailhouse

1,451 Views
Ahelion
Contributor IV

Hi all,

Is there any document showing all the steps to have a demo running on imx8qm mek board with jailhouse?

I was going over this: L5.4.70_2.3.3_LINUX_DOCS

but all I could find is a reference to device trees:

Hypervisor Jailhouse Enables the Jailhouse Hypervisor device trees.
• imx8qxp-mek-root.dtb: DTB for root-cell

I do not know what to do with this info. That is why I need a step by step instruction list.

Br, Mircea

 

Tags (1)
0 Kudos
Reply
7 Replies

1,431 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version BSP are you want to use?

0 Kudos
Reply

1,427 Views
Ahelion
Contributor IV

L5.4.70_2.3.3, i was following this quide, so all bsp-s mentioned here I am using.

0 Kudos
Reply

1,424 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

OK, I will help confirm.

0 Kudos
Reply

1,340 Views
Ahelion
Contributor IV

any ideea? 

Found out that the latest linux kernel does support the lates XEN

How can I get Linux and Android running at the same time?

 

0 Kudos
Reply

1,322 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

Yes, the xen is supported on the i.MX8QM.

You can refer to the attach document.

Wish you have a nice day

Best Regards

Rita

0 Kudos
Reply

1,316 Views
Ahelion
Contributor IV
I can tell you right now, it is not supported. I could not get jailhouse or xen to work on imx8qm. Whatever documentation i find is referencing linux4.9, which can not be build anymore.
0 Kudos
Reply

820 Views
Jerry137207
Contributor I

Hi, Ahelion:

I'm interested in runing multiple OS based on jailhouse, but related information is lack. I've sucessfully run jailhouse test demo in Imx8qm mek board. If you would like share info each other, plz email me: 1372071341@qq.com.

0 Kudos
Reply