imx8qm Galcore issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8qm Galcore issue

1,418 Views
songhongliang
Contributor II

HI,

[ 3.337967] usbcore: registered new interface driver usbhid
[ 3.343632] usbhid: USB HID core driver
[ 3.350312] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[ 3.357517] mxc-isi 58110000.isi: mxc_isi.1 registered successfully
[ 3.364667] mxc-isi 58120000.isi: mxc_isi.2 registered successfully
[ 3.371702] mxc-isi 58130000.isi: mxc_isi.3 registered successfully
[ 3.378712] mxc-isi 58140000.isi: mxc_isi.4 registered successfully
[ 3.385638] mxc-isi 58150000.isi: mxc_isi.5 registered successfully
[ 3.392052] mmc0: Command Queue Engine enabled
[ 3.392573] mxc-isi 58160000.isi: mxc_isi.6 registered successfully
[ 3.396566] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[ 3.403452] mxc-isi 58170000.isi: mxc_isi.7 registered successfully
[ 3.409860] mmcblk0: mmc0:0001 HAG4a2 14.7 GiB
[ 3.420461] mmcblk0boot0: mmc0:0001 HAG4a2 partition 1 8.00 MiB
[ 3.426507] mmcblk0boot1: mmc0:0001 HAG4a2 partition 2 8.00 MiB
[ 3.432604] mmcblk0rpmb: mmc0:0001 HAG4a2 partition 3 4.00 MiB, chardev (237:0)
[ 3.438706] mxc-mipi-csi2 58227000.csi: lanes: 4, name: mxc-mipi-csi2.0
[ 3.446627] mmcblk0: p1 p2
[ 3.466701] mxc-mipi-csi2 58247000.csi: lanes: 4, name: mxc-mipi-csi2.1
[ 3.477652] No fsl,qman node
[ 3.480581] Freescale USDPAA process driver
[ 3.484882] fsl-usdpaa: no region found
[ 3.489031] Freescale USDPAA process IRQ driver
[ 3.496457] imx-rproc imx8qm_cm4@0: failed to find syscon
[ 3.501936] remoteproc remoteproc0: releasing imx-rproc
[ 3.507289] imx-rproc imx8x_cm4@1: failed to find syscon
[ 3.512669] remoteproc remoteproc0: releasing imx-rproc
[ 3.520609] ddr_perf_probe:763 shl songhl
[ 3.524962] ddr_perf_probe:763 shl songhl
[ 3.539428] shl Galcore version 6.4.3.p0.286725
[ 3.543990] drv_init:1075 shl songhl

 

My kernel stops at Galcore and does not continue ,

use imx8qm , 2GB LPDDR4.

tftp 0x80280000 Image; tftp 0x83000000 imx8qm-mek.dtb; booti 0x80280000 - 0x83000000.

the lpddr4 Stress Test is success

Tags (1)
0 Kudos
Reply
4 Replies

1,413 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello songhongliang,

 

It look like we have a problem in 5.4.47 BSP It will be reported, the galcore tries to jump to a non memory localization, in the meantime use the kernel 5.4.24.

 

Regards

 

0 Kudos
Reply

1,407 Views
songhongliang
Contributor II

Hi,

How can I solve this problem

 

Regards

0 Kudos
Reply

1,398 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello

 

You have to update your kernel and build for your memory.

 

Regards

 

0 Kudos
Reply

1,388 Views
songhongliang
Contributor II

HI,

I am using the latest 5.4.47 kernel version,and use scfw ,And updated lpddr4 with scfw.the lpddr4 is  SKhynix  H9HCNNN8KUMLHR.Does dts also need to be modified?

Regards

0 Kudos
Reply